ModelUpdateSensitivityViewerBuilder Class¶
-
class
NXOpen.CAE.
ModelUpdateSensitivityViewerBuilder
¶ Bases:
NXOpen.Builder
Represents
NXOpen.CAE.ModelUpdateSensitivityViewerBuilder
To create a new instance of this class, use
NXOpen.CAE.ModelUpdateSolutionCollection.CreateSensitivityViewerBuilder
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDesignVariableLabels | Gets the design variable labels @return SM allocated array containing the design variable labels |
GetObject | Returns the object currently being edited by this builder. |
GetSensitivityValues | Gets the sensitivity values @return SM allocated array containing the sensitivity values |
GetTargetIds | Gets the target IDs |
SetDesignVariableLabels | Sets the design variable labels |
SetSensitivityValues | Sets the sensitivity values |
SetTargetIds | Sets the terget IDs |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetDesignVariableLabels¶
-
ModelUpdateSensitivityViewerBuilder.
GetDesignVariableLabels
¶ Gets the design variable labels
Signature
GetDesignVariableLabels()
Returns: SM allocated array containing the design variable labels Return type: list of str New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
GetSensitivityValues¶
-
ModelUpdateSensitivityViewerBuilder.
GetSensitivityValues
¶ Gets the sensitivity values
Signature
GetSensitivityValues()
Returns: SM allocated array containing the sensitivity values Return type: list of float New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
GetTargetIds¶
-
ModelUpdateSensitivityViewerBuilder.
GetTargetIds
¶ Gets the target IDs
Signature
GetTargetIds()
Returns: SM allocated array containing the targets ID Return type: list of int New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
SetDesignVariableLabels¶
-
ModelUpdateSensitivityViewerBuilder.
SetDesignVariableLabels
¶ Sets the design variable labels
Signature
SetDesignVariableLabels(designVaraibleLabels)
Parameters: designVaraibleLabels (list of str) – The design variable labels NOTE: The full Unicode character set is not supported for this parameter. New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
SetSensitivityValues¶
-
ModelUpdateSensitivityViewerBuilder.
SetSensitivityValues
¶ Sets the sensitivity values
Signature
SetSensitivityValues(sensitivityValues)
Parameters: sensitivityValues (list of float) – The sensitivity values New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
SetTargetIds¶
-
ModelUpdateSensitivityViewerBuilder.
SetTargetIds
¶ Sets the terget IDs
Signature
SetTargetIds(targetIds)
Parameters: targetIds (list of int) – The target IDs New in version NX6.0.0.
License requirements: nx_correl_update (“FE Model Update”)
Validate¶
-
ModelUpdateSensitivityViewerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.