SimSolutionSetupCheckOption Enumeration¶
NXOpen.CAE.SimSolution.SetupCheckOption is an alias for NXOpen.CAE.SimSolutionSetupCheckOption
-
class
NXOpen.CAE.
SimSolutionSetupCheckOption
¶ Bases:
object
Model Setup Check Options
Enum Members
Enum Member Enum Member Description DoNotCheck do perform any set up checksCheckAndStopAtFirstError perform set up checks but stop at first errorCompleteCheckAndOutputErrors perform all set up checks and report all errors-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-