SimBcXyPlotBuilder Class¶
-
class
NXOpen.CAE.
SimBcXyPlotBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.SimBcXyPlotBuilder
builder which can be used to generate a XY plot of aNXOpen.CAE.SimBC
in the graphics area.This is limited to
NXOpen.CAE.SimBC
objects in the active solution. To create a new instance of this class, useNXOpen.CAE.SimSimulation.CreateSimBcXyPlotBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
MultipleMatches | Returns or sets a NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches used in plot to resolve multiple values |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAvailableBcsToPlot | Returns all available NXOpen.CAE.SimBC to plot @return |
GetAvailablePropertyNamesToPlot | Returns all available property names that can be plotted for the specified NXOpen.CAE.SimBC @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
Plot | Creates XY plot @return Created plot |
SetBcsToPlot | Sets NXOpen.CAE.SimBC objects to plot. |
SetLocationElement | Sets location at an element |
SetLocationElementEdge | Sets location at an element edge |
SetLocationElementFace | Sets location at an element face |
SetLocationNode | Sets location at a node |
SetPropertyNameToPlot | Sets property name to plot. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SimBcXyPlotBuilderResolveMultipleMatches Enumeration | Resolve multiple matches when the location specified matches multiple items in the boundary condition’s target set |
Property Detail¶
MultipleMatches¶
-
SimBcXyPlotBuilder.
MultipleMatches
¶ Returns or sets a
NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches
used in plot to resolve multiple values-------------------------------------
Getter Method
Signature
MultipleMatches()
Returns: Return type: NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
MultipleMatches(resolveMultipleMatches)
Parameters: resolveMultipleMatches ( NXOpen.CAE.SimBcXyPlotBuilderResolveMultipleMatches
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetAvailableBcsToPlot¶
-
SimBcXyPlotBuilder.
GetAvailableBcsToPlot
¶ Returns all available
NXOpen.CAE.SimBC
to plotSignature
GetAvailableBcsToPlot()
Returns: Return type: list of NXOpen.CAE.SimBC
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetAvailablePropertyNamesToPlot¶
-
SimBcXyPlotBuilder.
GetAvailablePropertyNamesToPlot
¶ Returns all available property names that can be plotted for the specified
NXOpen.CAE.SimBC
Signature
GetAvailablePropertyNamesToPlot(tBc)
Parameters: tBc ( NXOpen.CAE.SimBC
) –Returns: Return type: list of str New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Plot¶
-
SimBcXyPlotBuilder.
Plot
¶ Creates XY plot
Signature
Plot(deviceIndex, viewIndex)
Parameters: - deviceIndex (int) – device index
- viewIndex (int) – view index
Returns: Created plot
Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetBcsToPlot¶
-
SimBcXyPlotBuilder.
SetBcsToPlot
¶ Overloaded method SetBcsToPlot
SetBcsToPlot(bcs, propertyNames)
SetBcsToPlot(bcs)
-------------------------------------
Sets
NXOpen.CAE.SimBC
objects to plot.Signature
SetBcsToPlot(bcs, propertyNames)
Parameters: - bcs (list of
NXOpen.CAE.SimBC
) – boundary conditions to plot - propertyNames (list of str) – property names to plot NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Sets
NXOpen.CAE.SimBC
objects to plot.Signature
SetBcsToPlot(bcs)
Parameters: bcs (list of NXOpen.CAE.SimBC
) – boundary conditions to plotNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
SetLocationElement¶
-
SimBcXyPlotBuilder.
SetLocationElement
¶ Sets location at an element
Signature
SetLocationElement(element)
Parameters: element ( NXOpen.CAE.FEElement
) – elementNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetLocationElementEdge¶
-
SimBcXyPlotBuilder.
SetLocationElementEdge
¶ Sets location at an element edge
Signature
SetLocationElementEdge(elementEdge)
Parameters: elementEdge ( NXOpen.CAE.FEElemEdge
) – element edgeNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetLocationElementFace¶
-
SimBcXyPlotBuilder.
SetLocationElementFace
¶ Sets location at an element face
Signature
SetLocationElementFace(elementFace)
Parameters: elementFace ( NXOpen.CAE.FEElemFace
) – element faceNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetLocationNode¶
-
SimBcXyPlotBuilder.
SetLocationNode
¶ Sets location at a node
Signature
SetLocationNode(node)
Parameters: node ( NXOpen.CAE.FENode
) – nodeNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetPropertyNameToPlot¶
-
SimBcXyPlotBuilder.
SetPropertyNameToPlot
¶ Sets property name to plot.
Signature
SetPropertyNameToPlot(pPropertyName)
Parameters: pPropertyName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
SimBcXyPlotBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.