LaminateImportZonesBuilder Class¶
-
class
NXOpen.CAE.
LaminateImportZonesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateImportZonesBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLaminateImportZonesBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Filename | Returns or sets the full name and path of the file to be imported |
ImportBoundaries | Returns or sets the boundaries import option |
ImportMaterials | Returns or sets the material import option |
OverwriteCollectors | Returns or sets the mesh collectors overwrite option |
OverwriteLamProps | Returns or sets the laminate properties overwrite option |
OverwriteMaterials | Returns or sets the material import overwrite option |
SearchDistance | Returns the search distance used to localize each FEM element in the FiberSIM zone mesh |
Selection | Returns the geometric face(s) and element face(s) on which to zones will be imported |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Filename¶
-
LaminateImportZonesBuilder.
Filename
¶ Returns or sets the full name and path of the file to be imported
-------------------------------------
Getter Method
Signature
Filename()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Filename(filename)
Parameters: filename (str) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ImportBoundaries¶
-
LaminateImportZonesBuilder.
ImportBoundaries
¶ Returns or sets the boundaries import option
-------------------------------------
Getter Method
Signature
ImportBoundaries()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportBoundaries(importBoundaries)
Parameters: importBoundaries (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ImportMaterials¶
-
LaminateImportZonesBuilder.
ImportMaterials
¶ Returns or sets the material import option
-------------------------------------
Getter Method
Signature
ImportMaterials()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportMaterials(importMaterials)
Parameters: importMaterials (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
OverwriteCollectors¶
-
LaminateImportZonesBuilder.
OverwriteCollectors
¶ Returns or sets the mesh collectors overwrite option
-------------------------------------
Getter Method
Signature
OverwriteCollectors()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverwriteCollectors(overwriteCollectors)
Parameters: overwriteCollectors (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
OverwriteLamProps¶
-
LaminateImportZonesBuilder.
OverwriteLamProps
¶ Returns or sets the laminate properties overwrite option
-------------------------------------
Getter Method
Signature
OverwriteLamProps()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverwriteLamProps(overwriteLamProps)
Parameters: overwriteLamProps (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
OverwriteMaterials¶
-
LaminateImportZonesBuilder.
OverwriteMaterials
¶ Returns or sets the material import overwrite option
-------------------------------------
Getter Method
Signature
OverwriteMaterials()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverwriteMaterials(overwriteMaterials)
Parameters: overwriteMaterials (bool) – New in version NX10.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
SearchDistance¶
-
LaminateImportZonesBuilder.
SearchDistance
¶ Returns the search distance used to localize each FEM element in the FiberSIM zone mesh
-------------------------------------
Getter Method
Signature
SearchDistance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Selection¶
-
LaminateImportZonesBuilder.
Selection
¶ Returns the geometric face(s) and element face(s) on which to zones will be imported
-------------------------------------
Getter Method
Signature
Selection()
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LaminateImportZonesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.