SimConditionTimeStepCollection Class¶
-
class
NXOpen.CAE.
SimConditionTimeStepCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.SimConditionTimeStep
.To obtain an instance of this class, refer to
NXOpen.CAE.SimConditionSequence
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates a NXOpen.CAE.SimConditionTimeStep at specified time referencing specified NXOpen.CAE.SimCondition and insert it in time history. |
Delete | Deletes a NXOpen.CAE.SimConditionTimeStep from time history |
Find | Collection’s object finder @return The NXOpen.CAE.SimConditionTimeStep |
Get | Returns the NXOpen.CAE.SimConditionTimeStep at the specified time or None if it doesn’t exist @return the corresponding NXOpen.CAE.SimConditionTimeStep |
GetAll | Returns a time ordered array of all NXOpen.CAE.SimConditionTimeStep @return all NXOpen.CAE.SimConditionTimeStep |
GetInRange | Returns all NXOpen.CAE.SimConditionTimeStep falling inside the specified inclusive time range @return all NXOpen.CAE.SimConditionTimeStep within range |
GetWithReferenceToCondition | Returns all NXOpen.CAE.SimConditionTimeStep referencing the specified NXOpen.CAE.SimCondition @return all NXOpen.CAE.SimConditionTimeStep referencing specified NXOpen.CAE.SimCondition |
ModifyTime | Modifies the time of a NXOpen.CAE.SimConditionTimeStep in time history |
Method Detail¶
Create¶
-
SimConditionTimeStepCollection.
Create
¶ Creates a
NXOpen.CAE.SimConditionTimeStep
at specified time referencing specifiedNXOpen.CAE.SimCondition
and insert it in time history.A conditionless
NXOpen.CAE.SimConditionTimeStep
may be added by passing None as theNXOpen.CAE.SimCondition
.Signature
Create(time, condition, description)
Parameters: - time (float) –
- condition (
NXOpen.CAE.SimCondition
) – - description (str) – NOTE: The full Unicode character set is not supported for this parameter.
Returns: the added Time Step
NXOpen.CAE.SimConditionTimeStep
Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Delete¶
-
SimConditionTimeStepCollection.
Delete
¶ Deletes a
NXOpen.CAE.SimConditionTimeStep
from time historySignature
Delete(step)
Parameters: step ( NXOpen.CAE.SimConditionTimeStep
) –New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Find¶
-
SimConditionTimeStepCollection.
Find
¶ Collection’s object finder
Signature
Find(time)
Parameters: time (str) – time of the NXOpen.CAE.SimConditionTimeStep
Returns: The NXOpen.CAE.SimConditionTimeStep
Return type: NXOpen.CAE.SimConditionTimeStep
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Get¶
-
SimConditionTimeStepCollection.
Get
¶ Returns the
NXOpen.CAE.SimConditionTimeStep
at the specified time or None if it doesn’t existSignature
Get(time)
Parameters: time (float) – Returns: the corresponding NXOpen.CAE.SimConditionTimeStep
Return type: NXOpen.CAE.SimConditionTimeStep
New in version NX9.0.0.
License requirements: None.
GetAll¶
-
SimConditionTimeStepCollection.
GetAll
¶ Returns a time ordered array of all
NXOpen.CAE.SimConditionTimeStep
Signature
GetAll()
Returns: all NXOpen.CAE.SimConditionTimeStep
Return type: list of NXOpen.CAE.SimConditionTimeStep
New in version NX9.0.0.
License requirements: None.
GetInRange¶
-
SimConditionTimeStepCollection.
GetInRange
¶ Returns all
NXOpen.CAE.SimConditionTimeStep
falling inside the specified inclusive time rangeSignature
GetInRange(fromTime, toTime)
Parameters: - fromTime (float) –
- toTime (float) –
Returns: all
NXOpen.CAE.SimConditionTimeStep
within rangeReturn type: list of
NXOpen.CAE.SimConditionTimeStep
New in version NX9.0.0.
License requirements: None.
GetWithReferenceToCondition¶
-
SimConditionTimeStepCollection.
GetWithReferenceToCondition
¶ Returns all
NXOpen.CAE.SimConditionTimeStep
referencing the specifiedNXOpen.CAE.SimCondition
Signature
GetWithReferenceToCondition(condition)
Parameters: condition ( NXOpen.CAE.SimCondition
) –Returns: all NXOpen.CAE.SimConditionTimeStep
referencing specifiedNXOpen.CAE.SimCondition
Return type: list of NXOpen.CAE.SimConditionTimeStep
New in version NX9.0.0.
License requirements: None.
ModifyTime¶
-
SimConditionTimeStepCollection.
ModifyTime
¶ Modifies the time of a
NXOpen.CAE.SimConditionTimeStep
in time historySignature
ModifyTime(step, time)
Parameters: - step (
NXOpen.CAE.SimConditionTimeStep
) – - time (float) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- step (