NodeAlignBuilder Class¶
-
class
NXOpen.CAE.
NodeAlignBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodeAlignBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodeAlignBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
MidNodeMove | Returns or sets the mid node move |
Node | Returns the node |
Point1 | Returns the point1 of line |
Point2 | Returns the point2 of line |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
MidNodeMove¶
-
NodeAlignBuilder.
MidNodeMove
¶ Returns or sets the mid node move
-------------------------------------
Getter Method
Signature
MidNodeMove()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MidNodeMove(midNodeMove)
Parameters: midNodeMove (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
NodeAlignBuilder.
Node
¶ Returns the node
-------------------------------------
Getter Method
Signature
Node()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX5.0.0.
License requirements: None.
Point1¶
-
NodeAlignBuilder.
Point1
¶ Returns the point1 of line
-------------------------------------
Getter Method
Signature
Point1()
Returns: Return type: NXOpen.CAE.SelectFENode
New in version NX5.0.0.
License requirements: None.
Point2¶
-
NodeAlignBuilder.
Point2
¶ Returns the point2 of line
-------------------------------------
Getter Method
Signature
Point2()
Returns: Return type: NXOpen.CAE.SelectFENode
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
NodeAlignBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.