ReassignElementsBuilderElementDimensionOption Enumeration¶
NXOpen.CAE.ReassignElementsBuilder.ElementDimensionOption is an alias for NXOpen.CAE.ReassignElementsBuilderElementDimensionOption
-
class
NXOpen.CAE.
ReassignElementsBuilderElementDimensionOption
¶ Bases:
object
Indicates the different element dimensions
Enum Members
Enum Member Enum Member Description Point 0-dBeam 1-dShell 2-dSolid 3-d-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-