PropertyTablePropertyType Enumeration¶
NXOpen.CAE.PropertyTable.PropertyType is an alias for NXOpen.CAE.PropertyTablePropertyType
-
class
NXOpen.CAE.
PropertyTablePropertyType
¶ Bases:
object
Property Types
Enum Members
Enum Member Enum Member Description Unknown BASE_PROPERTY_TABLE_property_type_unknownString BASE_PROPERTY_TABLE_property_type_stringBoolean BASE_PROPERTY_TABLE_property_type_booleanInteger BASE_PROPERTY_TABLE_property_type_integerDouble BASE_PROPERTY_TABLE_property_type_doubleFieldWrapper BASE_PROPERTY_TABLE_property_type_field_wrapperScalarFieldWrapper BASE_PROPERTY_TABLE_property_type_scalar_field_wrapperCoordinateSystem BASE_PROPERTY_TABLE_property_type_coordinate_systemDoubleArray BASE_PROPERTY_TABLE_property_type_double_arrayIntegerArray BASE_PROPERTY_TABLE_property_type_integer_arrayPhysicalMaterial BASE_PROPERTY_TABLE_property_type_physical_materialMatrix BASE_PROPERTY_TABLE_property_type_matrixScalarTable BASE_PROPERTY_TABLE_property_type_scalar_tableText FieldExpression VectorFieldWrapper Vector Reference Point DateTime NamedPropertyTableArray SetManager NamedPropertyTable Axis CaeSection SectionOrientation SectionOffset -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-