AfuMathOperationOverall Enumeration¶
NXOpen.CAE.AfuMathOperation.Overall is an alias for NXOpen.CAE.AfuMathOperationOverall
-
class
NXOpen.CAE.
AfuMathOperationOverall
¶ Bases:
object
Defines the type of Overall Math Operations
Enum Members
Enum Member Enum Member Description MinimumValue Gets minimum values of AFU recordsMaximumValue Gets maximum values of AFU recordsMinimumMagnitude Gets minimum magnitude values of AFU recordsMaximumMagnitude Gets maximum magnitude values of AFU recordsMeanMagnitude Gets mean magnitude values of AFU recordsSumMagnitude Gets sum magnitude values of AFU recordsSumComplex Gets complex sum values of AFU records-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-