ResultLoadcaseValueType Enumeration¶
NXOpen.CAE.Result.LoadcaseValueType is an alias for NXOpen.CAE.ResultLoadcaseValueType
-
class
NXOpen.CAE.
ResultLoadcaseValueType
¶ Bases:
object
Value type for result load case
Enum Members
Enum Member Enum Member Description Unknown Unknown Value type Frequency Value type - Frequency LoadFactor Value type - Load Factor NodeDOF Value type - Node DOF LoadCase Value type - Load Case Time Value type - Time -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-