SimConditionParamCollection Class¶
-
class
NXOpen.CAE.
SimConditionParamCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.SimConditionParam
which represents a measurable environment.To obtain an instance of this class, refer to
NXOpen.CAE.SimConditionSeqMgr
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
Create | Creates a NXOpen.CAE.SimConditionParam with the specified name and units. |
Delete | Deletes a NXOpen.CAE.SimConditionParam . |
Find | Collection’s object finder @return The NXOpen.CAE.SimConditionParam |
Get | Returns the NXOpen.CAE.SimConditionParam with the specified name or None if such a parameter doesn’t exist @return the corresponding NXOpen.CAE.SimConditionParam |
GetAll | Returns all NXOpen.CAE.SimConditionParam @return all NXOpen.CAE.SimConditionParam |
Method Detail¶
Create¶
-
SimConditionParamCollection.
Create
¶ Creates a
NXOpen.CAE.SimConditionParam
with the specified name and units.Will error out if a
NXOpen.CAE.SimConditionParam
with specified name already exists. Specified name cannot be empty.Signature
Create(name, units)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- units (
NXOpen.Unit
) –
Returns: Created
NXOpen.CAE.SimConditionParam
Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Delete¶
-
SimConditionParamCollection.
Delete
¶ Deletes a
NXOpen.CAE.SimConditionParam
.All values in
NXOpen.CAE.SimCondition
for thatNXOpen.CAE.SimConditionParam
will also be deleted. Will return the number ofNXOpen.CAE.SimConditionParam
actually deleted.Signature
Delete(param)
Parameters: param ( NXOpen.CAE.SimConditionParam
) –Returns: Return type: int New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Find¶
-
SimConditionParamCollection.
Find
¶ Collection’s object finder
Signature
Find(name)
Parameters: name (str) – name of the NXOpen.CAE.SimConditionParam
Returns: The NXOpen.CAE.SimConditionParam
Return type: NXOpen.CAE.SimConditionParam
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Get¶
-
SimConditionParamCollection.
Get
¶ Returns the
NXOpen.CAE.SimConditionParam
with the specified name or None if such a parameter doesn’t existSignature
Get(name)
Parameters: name (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: the corresponding NXOpen.CAE.SimConditionParam
Return type: NXOpen.CAE.SimConditionParam
New in version NX9.0.0.
License requirements: None.
GetAll¶
-
SimConditionParamCollection.
GetAll
¶ Returns all
NXOpen.CAE.SimConditionParam
Signature
GetAll()
Returns: all NXOpen.CAE.SimConditionParam
Return type: list of NXOpen.CAE.SimConditionParam
New in version NX9.0.0.
License requirements: None.