SimConditionParam Class¶
-
class
NXOpen.CAE.
SimConditionParam
¶ Bases:
NXOpen.TaggedObject
This class represents a named measurable quantity. A collection of
NXOpen.CAE.SimConditionParam
represents a measurable environment. ANXOpen.CAE.SimCondition
consists of specified values for allNXOpen.CAE.SimConditionParam
, thus defining a state of the measurable environment.An instance of this class can be obtained from
NXOpen.CAE.SimConditionSeqMgr
.New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns the parameter name |
Tag | Returns the Tag for this object. |
Units | Returns the parameter units |
Methods¶
Method | Description |
---|---|
Modify | Modifies the name and units of NXOpen.CAE.SimConditionParam . |
Property Detail¶
Name¶
-
SimConditionParam.
Name
¶ Returns the parameter name
-------------------------------------
Getter Method
Signature
Name()
Returns: the name value Return type: str New in version NX9.0.0.
License requirements: None.
Units¶
-
SimConditionParam.
Units
¶ Returns the parameter units
-------------------------------------
Getter Method
Signature
Units()
Returns: the units value Return type: NXOpen.Unit
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Modify¶
-
SimConditionParam.
Modify
¶ Modifies the name and units of
NXOpen.CAE.SimConditionParam
.An error will be issued if new name clashes with existing
NXOpen.CAE.SimConditionParam
. Measure of units cannot be modified.Signature
Modify(name, units)
Parameters: - name (str) – NOTE: The full Unicode character set is not supported for this parameter.
- units (
NXOpen.Unit
) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)