DurabilityFatigueCollection Class¶
-
class
NXOpen.CAE.
DurabilityFatigueCollection
¶ Bases:
object
Represents a collection of event fatigue settings.
To obtain an instance of this class, refer to
NXOpen.CAE.DurabilityManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CloneFatigue | Clones a durability event fatigue settings. |
CreateEventfatiguesettingsBuilder | Creates the builder object of durability event fatigue settings. |
DeleteFatigue | Delete a durability fatigue. |
FindObject | Finds an event fatigue settings with a specified name. |
Method Detail¶
CloneFatigue¶
-
DurabilityFatigueCollection.
CloneFatigue
¶ Clones a durability event fatigue settings.
Signature
CloneFatigue(source)
Parameters: source ( NXOpen.CAE.DurabilityFatigue
) – Source event fatigue settingssReturns: Cloned event fatigue settingss Return type: NXOpen.CAE.DurabilityFatigue
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CreateEventfatiguesettingsBuilder¶
-
DurabilityFatigueCollection.
CreateEventfatiguesettingsBuilder
¶ Creates the builder object of durability event fatigue settings.
Signature
CreateEventfatiguesettingsBuilder(eventfatiguesettings)
Parameters: eventfatiguesettings ( NXOpen.CAE.DurabilityFatigue
) –Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilder
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
DeleteFatigue¶
-
DurabilityFatigueCollection.
DeleteFatigue
¶ Delete a durability fatigue.
Signature
DeleteFatigue(eventfatiguesettings)
Parameters: eventfatiguesettings ( NXOpen.CAE.DurabilityFatigue
) – The durability event fatigue settings to be deletedNew in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FindObject¶
-
DurabilityFatigueCollection.
FindObject
¶ Finds an event fatigue settings with a specified name.
Signature
FindObject(name)
Parameters: name (str) – name of the durability event fatigue settings Returns: The durability event fatigue settings Return type: NXOpen.CAE.DurabilityFatigue
New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)