DurabilityEventStrengthSettingsBuilderStressTypeEnum Enumeration¶
NXOpen.CAE.DurabilityEventStrengthSettingsBuilder.StressTypeEnum is an alias for NXOpen.CAE.DurabilityEventStrengthSettingsBuilderStressTypeEnum
-
class
NXOpen.CAE.
DurabilityEventStrengthSettingsBuilderStressTypeEnum
¶ Bases:
object
the stress type enum.
Enum Members
Enum Member Enum Member Description VonMises Von MisesTresca TrescaMaximumPrincipal Maximum PrincipalMinimumPrincipal Minimum Principal-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-