XyFunctionMeasure Enumeration¶
-
class
NXOpen.CAE.
XyFunctionMeasure
¶ Bases:
object
Defines measurement unit types Enum Members
Enum Member Enum Member Description General General unitDisplacement Displacement unitForce Force unitTemperature Temperature unitTime Time unitFrequency Frequency unitMass Mass unitVelocity Velocity unitAcceleration Acceleration unitAngularDisplacement Angular displacement unitAngularVelocity Angular velocity unitAngularAcceleration Angular acceleration unitMoment Moment unitPressure Pressure unitStress Stress unitStrain Strain unitRpm RPM unitOrder Order unitCycles Cycles unitLoadfactor Load Factor unitTorque Torque unitGravity Gravity unitCurvature Curvature unitElementForce Element force unitElementMoment Element moment unitMotorSignal Motor signal unitUnitlessScalar Unitless scalar unitUnitlessReal Unitless real unitUnitlessInteger Unitless integer unitVoltage Voltage unitElectricCurrent Electric current unitNumber Measure number-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-