MeshCollectorBuilder Class¶
-
class
NXOpen.CAE.
MeshCollectorBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MeshCollectorBuilder
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateCollectorBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CollectorName | Returns or sets the collector name |
PropertyTable | Returns the Mesh Collector’s Property Table |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MeshCollectorBuilderElementDimensionOption Enumeration | Indicates the different element dimensions |
Property Detail¶
CollectorName¶
-
MeshCollectorBuilder.
CollectorName
¶ Returns or sets the collector name
-------------------------------------
Getter Method
Signature
CollectorName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollectorName(collectorName)
Parameters: collectorName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PropertyTable¶
-
MeshCollectorBuilder.
PropertyTable
¶ Returns the Mesh Collector’s Property Table
-------------------------------------
Getter Method
Signature
PropertyTable()
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MeshCollectorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.