CfdContactPreventionConstraint Class¶
-
class
NXOpen.CAE.
CfdContactPreventionConstraint
¶ Bases:
NXOpen.TaggedObject
The contact prevention constraint is a type of constraint which is used by the Fluid Domain Recipe to generate a fluid domain.
To create or edit an instance of this class, use
NXOpen.CAE.CfdContactPreventionConstraintBuilder
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
GetName | Gets the name of the contact prevention constraint @return |
SetName | Sets the name of the contact prevention constraint |