PreTestSensorConfigCollection Class¶
-
class
NXOpen.CAE.
PreTestSensorConfigCollection
¶ Bases:
object
Represents a collection of sensor selection configuration
To obtain an instance of this class, refer to
NXOpen.CAE.PreTestSensorSelectionControl
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ActiveSensorConfig | Returns or sets the pre-test active sensor configuration |
Methods¶
Method | Description |
---|---|
CloneSensorConfig | Clone a pre-test sensor configuration @return Cloned Pre-Test sensor configuration |
FindObject | Finds a sensor selection configuration with specified name @return sensor selection configuration found |
RemoveSensorConfig | Removes and deletes a sensor selection configuration |
Property Detail¶
ActiveSensorConfig¶
-
PreTestSensorConfigCollection.
ActiveSensorConfig
¶ Returns or sets the pre-test active sensor configuration
-------------------------------------
Getter Method
Signature
ActiveSensorConfig()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveSensorConfig(activeConfig)
Parameters: activeConfig (int) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
CloneSensorConfig¶
-
PreTestSensorConfigCollection.
CloneSensorConfig
¶ Clone a pre-test sensor configuration
Signature
CloneSensorConfig(source)
Parameters: source ( NXOpen.CAE.PreTestSensorConfig
) – Pre-Test sensor configuration to be clonedReturns: Cloned Pre-Test sensor configuration Return type: NXOpen.CAE.PreTestSensorConfig
New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
FindObject¶
-
PreTestSensorConfigCollection.
FindObject
¶ Finds a sensor selection configuration with specified name
Signature
FindObject(name)
Parameters: name (str) – sensor selection configuration name to be found Returns: sensor selection configuration found Return type: NXOpen.CAE.PreTestSensorConfig
New in version NX7.5.0.
License requirements: None.
RemoveSensorConfig¶
-
PreTestSensorConfigCollection.
RemoveSensorConfig
¶ Removes and deletes a sensor selection configuration
Signature
RemoveSensorConfig(toRemove)
Parameters: toRemove (int) – Index of the sensor selection configuration to remove New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)