BushingEADBuilder Class¶
-
class
NXOpen.CAE.
BushingEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Bushing Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateBushingEadBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the select element operator selects elements |
OriCsystem | Returns or sets the get coordinate system method gets the coordinate system for orienting by coordinate system |
OriDirr | Returns or sets the get oriDirr operator gets orientaion vector value |
OriMethod | Returns or sets the method to get the element orientation method |
OriNode | Returns the get ori_node operator selects an orientation node |
OrientationState | Returns or sets the state drives the commit action |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BushingEADBuilderOrientationMethod Enumeration | indicates which orientation method to use |
BushingEADBuilderState Enumeration | indicates to ignore, apply or clear the state property upon commit |
Property Detail¶
Elements¶
-
BushingEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriCsystem¶
-
BushingEADBuilder.
OriCsystem
¶ Returns or sets the get coordinate system method gets the coordinate system for orienting by coordinate system
-------------------------------------
Getter Method
Signature
OriCsystem()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OriCsystem(oriCsystem)
Parameters: oriCsystem ( NXOpen.CoordinateSystem
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriDirr¶
-
BushingEADBuilder.
OriDirr
¶ Returns or sets the get oriDirr operator gets orientaion vector value
-------------------------------------
Getter Method
Signature
OriDirr()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OriDirr(oriDirr)
Parameters: oriDirr ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriMethod¶
-
BushingEADBuilder.
OriMethod
¶ Returns or sets the method to get the element orientation method
-------------------------------------
Getter Method
Signature
OriMethod()
Returns: Return type: NXOpen.CAE.BushingEADBuilderOrientationMethod
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OriMethod(oriMethod)
Parameters: oriMethod ( NXOpen.CAE.BushingEADBuilderOrientationMethod
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriNode¶
-
BushingEADBuilder.
OriNode
¶ Returns the get ori_node operator selects an orientation node
-------------------------------------
Getter Method
Signature
OriNode()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OrientationState¶
-
BushingEADBuilder.
OrientationState
¶ Returns or sets the state drives the commit action
-------------------------------------
Getter Method
Signature
OrientationState()
Returns: Return type: NXOpen.CAE.BushingEADBuilderState
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OrientationState(orientationState)
Parameters: orientationState ( NXOpen.CAE.BushingEADBuilderState
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
BushingEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.