ShellEADBuilderState Enumeration¶
NXOpen.CAE.ShellEADBuilder.State is an alias for NXOpen.CAE.ShellEADBuilderState
-
class
NXOpen.CAE.
ShellEADBuilderState
¶ Bases:
object
indicates to ignore, apply or clear the state property upon commit
Enum Members
Enum Member Enum Member Description Ignore do nothing to the propertyApply apply the propertyClear clear the property-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-