CAEWeldConnectionBuilderWeldTypeEnum Enumeration¶
NXOpen.CAE.CAEWeldConnectionBuilder.WeldTypeEnum is an alias for NXOpen.CAE.CAEWeldConnectionBuilderWeldTypeEnum
-
class
NXOpen.CAE.
CAEWeldConnectionBuilderWeldTypeEnum
¶ Bases:
object
the type of weld connection to be created
Enum Members
Enum Member Enum Member Description PointToPointDirect It’s a point to point direct weldconnection,mesh points are created during weld connectionPointToPointIndirect It’s a point to point in-direct weldconnection,RBE3 elements are created during weld connectionPointToPoint3dWeld It’s a point to point in-direct weldconnection,3D elements are created during weld connection-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-