LaminateLayupOffsetBuilder Class¶
-
class
NXOpen.CAE.
LaminateLayupOffsetBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateLayupOffset
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLayupOffsetBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
FiberDistance | Returns or sets the fiber distance |
RefPlanePosition | Returns the reference plane position expression |
Selection | Returns the geometric face(s) and element faces on which to assign the layup offset rule |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FiberDistance¶
-
LaminateLayupOffsetBuilder.
FiberDistance
¶ Returns or sets the fiber distance
-------------------------------------
Getter Method
Signature
FiberDistance()
Returns: Return type: float New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateLayupOffsetBuilder.RefPlanePosition
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
-------------------------------------
Setter Method
Signature
FiberDistance(fiberDistance)
Parameters: fiberDistance (float) – fiber distance New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.CAE.LaminateLayupOffsetBuilder.RefPlanePosition
instead.License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
RefPlanePosition¶
-
LaminateLayupOffsetBuilder.
RefPlanePosition
¶ Returns the reference plane position expression
-------------------------------------
Getter Method
Signature
RefPlanePosition()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Selection¶
-
LaminateLayupOffsetBuilder.
Selection
¶ Returns the geometric face(s) and element faces on which to assign the layup offset rule
-------------------------------------
Getter Method
Signature
Selection()
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX7.5.2.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
Validate¶
-
LaminateLayupOffsetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.