BeamEADBuilderVectorChoiceType Enumeration¶
NXOpen.CAE.BeamEADBuilder.VectorChoiceType is an alias for NXOpen.CAE.BeamEADBuilderVectorChoiceType
-
class
NXOpen.CAE.
BeamEADBuilderVectorChoiceType
¶ Bases:
object
indicates which vector choice to use
Enum Members
Enum Member Enum Member Description Horizontal the vector is defined to be horizontalVertical the vector is defined to be vertical-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-