BeamSectionOffsetOptionsMethod Enumeration¶
NXOpen.CAE.BeamSectionOffsetOptions.Method is an alias for NXOpen.CAE.BeamSectionOffsetOptionsMethod
-
class
NXOpen.CAE.
BeamSectionOffsetOptionsMethod
¶ Bases:
object
Represents the offset definition method
Enum Members
Enum Member Enum Member Description Neutral The offset coordindate system is defined in neutral wayLanguageSpecific The offset coordindate system is defined in language-specific way. Only available to Nastran-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-