PhysicalPropertyTableCollection Class¶
-
class
NXOpen.CAE.
PhysicalPropertyTableCollection
¶ Bases:
object
Creates physical property tables:py:class:NXOpen.CAE.PhysicalPropertyTable in a fem model
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CopyLaminatePropertyTableAs2d3d | Copies a Nastran Shell NXOpen.CAE.Laminate as a Nastran Solid NXOpen.CAE.Laminate , and vice versa. |
CopyPhysicalPropertyTable | Copies a NXOpen.CAE.PhysicalPropertyTable @return Physical property table copied |
CreatePhysicalPropertyTable | Creates a NXOpen.CAE.PhysicalPropertyTable @return Physical property table created |
FindObject | Finds the NXOpen.CAE.PhysicalPropertyTable with the given identifier as recorded in a journal. |
Method Detail¶
CopyLaminatePropertyTableAs2d3d¶
-
PhysicalPropertyTableCollection.
CopyLaminatePropertyTableAs2d3d
¶ Copies a Nastran Shell
NXOpen.CAE.Laminate
as a Nastran SolidNXOpen.CAE.Laminate
, and vice versa.Signature
CopyLaminatePropertyTableAs2d3d(sourceLaminate)
Parameters: sourceLaminate ( NXOpen.CAE.Laminate
) – Source laminate physical property to copyReturns: Copy of the source laminate physical property Return type: NXOpen.CAE.Laminate
New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CopyPhysicalPropertyTable¶
-
PhysicalPropertyTableCollection.
CopyPhysicalPropertyTable
¶ Copies a
NXOpen.CAE.PhysicalPropertyTable
Signature
CopyPhysicalPropertyTable(sourcePhysicalPropertyTable)
Parameters: sourcePhysicalPropertyTable ( NXOpen.CAE.PhysicalPropertyTable
) – Physical property table to copyReturns: Physical property table copied Return type: NXOpen.CAE.PhysicalPropertyTable
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreatePhysicalPropertyTable¶
-
PhysicalPropertyTableCollection.
CreatePhysicalPropertyTable
¶ Creates a
NXOpen.CAE.PhysicalPropertyTable
Signature
CreatePhysicalPropertyTable(descriptorType, languageName, solverName, name, label)
Parameters: - descriptorType (str) – Name of the physical property table descriptor NOTE: The full Unicode character set is not supported for this parameter.
- languageName (str) – language_name where to find the descriptor NOTE: The full Unicode character set is not supported for this parameter.
- solverName (str) – solver where to find the language NOTE: The full Unicode character set is not supported for this parameter.
- name (str) – Name of the physical property table NOTE: The full Unicode character set is not supported for this parameter.
- label (int) – Label for physical property table input 0 to get next available label
Returns: Physical property table created
Return type: New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
PhysicalPropertyTableCollection.
FindObject
¶ Finds the
NXOpen.CAE.PhysicalPropertyTable
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Physical property table found Return type: NXOpen.CAE.PhysicalPropertyTable
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)