LaminateImportedLayupBuilder Class¶
-
class
NXOpen.CAE.
LaminateImportedLayupBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LaminateImportedLayupBuilder
builderTo create a new instance of this class, use
NXOpen.CAE.LaminateGlobalLayupMgr.CreateLaminateImportedLayupBuilder
Default values.
Property Value FileType FiberSimXml ImportMethod ExternalFile NameOverride 0 Tolerance.Value 0 (millimeters part), 0 (inches part) New in version NX6.0.4.
Properties¶
Property | Description |
---|---|
ApiType | Returns or sets the external api selected for layup import |
FileName | Returns or sets the full name and path of the file to be imported |
FileType | Returns or sets the type of file to be imported |
ImportMaterials | Returns or sets the material import option |
ImportMethod | Returns or sets the import method |
LayupName | Returns or sets the user defined layup name |
NameOverride | Returns or sets the option to override the fibersim layup name with a user defined name |
OmitPartiallyMapped | Returns or sets the omit partially mapped face option. |
OverwriteMaterials | Returns or sets the material import overwrite option |
Selection | Returns the geometric face(s) and element face(s) on which to assign the material orientation |
Tag | Returns the Tag for this object. |
Tolerance | Returns the tolerance used to localize each FEM element layup information |
UnmappedFaceThreshold | Returns or sets the unmapped face threshold value (%). |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SelectLaminate | Selects a laminate for import |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateApiLaminateList | Updates the list of available laminates in the API |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LaminateImportedLayupBuilderApiTypeEnum Enumeration | Type of external API supported. |
LaminateImportedLayupBuilderFileEnum Enumeration | Type of external file to be imported. |
LaminateImportedLayupBuilderImportMethodEnum Enumeration | Import method type. |
Property Detail¶
ApiType¶
-
LaminateImportedLayupBuilder.
ApiType
¶ Returns or sets the external api selected for layup import
-------------------------------------
Getter Method
Signature
ApiType()
Returns: Return type: NXOpen.CAE.LaminateImportedLayupBuilderApiTypeEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApiType(apiType)
Parameters: apiType ( NXOpen.CAE.LaminateImportedLayupBuilderApiTypeEnum
) –New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FileName¶
-
LaminateImportedLayupBuilder.
FileName
¶ Returns or sets the full name and path of the file to be imported
-------------------------------------
Getter Method
Signature
FileName()
Returns: Return type: str New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName(filename)
Parameters: filename (str) – New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FileType¶
-
LaminateImportedLayupBuilder.
FileType
¶ Returns or sets the type of file to be imported
-------------------------------------
Getter Method
Signature
FileType()
Returns: Return type: NXOpen.CAE.LaminateImportedLayupBuilderFileEnum
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileType(fileType)
Parameters: fileType ( NXOpen.CAE.LaminateImportedLayupBuilderFileEnum
) –New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ImportMaterials¶
-
LaminateImportedLayupBuilder.
ImportMaterials
¶ Returns or sets the material import option
-------------------------------------
Getter Method
Signature
ImportMaterials()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportMaterials(importMaterials)
Parameters: importMaterials (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
ImportMethod¶
-
LaminateImportedLayupBuilder.
ImportMethod
¶ Returns or sets the import method
-------------------------------------
Getter Method
Signature
ImportMethod()
Returns: Return type: NXOpen.CAE.LaminateImportedLayupBuilderImportMethodEnum
New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportMethod(importMethod)
Parameters: importMethod ( NXOpen.CAE.LaminateImportedLayupBuilderImportMethodEnum
) –New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
LayupName¶
-
LaminateImportedLayupBuilder.
LayupName
¶ Returns or sets the user defined layup name
-------------------------------------
Getter Method
Signature
LayupName()
Returns: Return type: str New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayupName(layupName)
Parameters: layupName (str) – New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
NameOverride¶
-
LaminateImportedLayupBuilder.
NameOverride
¶ Returns or sets the option to override the fibersim layup name with a user defined name
-------------------------------------
Getter Method
Signature
NameOverride()
Returns: Return type: bool New in version NX6.0.4.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameOverride(nameOverride)
Parameters: nameOverride (bool) – New in version NX6.0.4.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
OmitPartiallyMapped¶
-
LaminateImportedLayupBuilder.
OmitPartiallyMapped
¶ Returns or sets the omit partially mapped face option.
When on, face(s) for which the number of elements successfully mapped in the FiberSim XML mesh is under a certain ratio, will be discarded.
-------------------------------------
Getter Method
Signature
OmitPartiallyMapped()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OmitPartiallyMapped(omitPartiallyMapped)
Parameters: omitPartiallyMapped (bool) – New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
OverwriteMaterials¶
-
LaminateImportedLayupBuilder.
OverwriteMaterials
¶ Returns or sets the material import overwrite option
-------------------------------------
Getter Method
Signature
OverwriteMaterials()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OverwriteMaterials(overwriteMaterials)
Parameters: overwriteMaterials (bool) – New in version NX8.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Selection¶
-
LaminateImportedLayupBuilder.
Selection
¶ Returns the geometric face(s) and element face(s) on which to assign the material orientation
-------------------------------------
Getter Method
Signature
Selection()
Returns: Return type: NXOpen.CAE.LaminateSelectEntitiesBuilder
New in version NX8.0.1.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Tolerance¶
-
LaminateImportedLayupBuilder.
Tolerance
¶ Returns the tolerance used to localize each FEM element layup information
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.4.
License requirements: None.
UnmappedFaceThreshold¶
-
LaminateImportedLayupBuilder.
UnmappedFaceThreshold
¶ Returns or sets the unmapped face threshold value (%).
When the OmitPartiallyMapped option is on, the percentage is used to determine which face(s) will be discarded during import.
-------------------------------------
Getter Method
Signature
UnmappedFaceThreshold()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnmappedFaceThreshold(unmappedFaceThreshold)
Parameters: unmappedFaceThreshold (float) – New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
SelectLaminate¶
-
LaminateImportedLayupBuilder.
SelectLaminate
¶ Selects a laminate for import
Signature
SelectLaminate(laminate)
Parameters: laminate (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
UpdateApiLaminateList¶
-
LaminateImportedLayupBuilder.
UpdateApiLaminateList
¶ Updates the list of available laminates in the API
Signature
UpdateApiLaminateList()
New in version NX8.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Validate¶
-
LaminateImportedLayupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.