SimLoadRecipeMapping Class¶
-
class
NXOpen.CAE.
SimLoadRecipeMapping
¶ Bases:
NXOpen.TaggedObject
This is the class handling the mapping of a certain load type of a load recipe.
Mappings are unique for each load type, thus one cannot be created
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
LoadType | Returns the load type of a NXOpen.CAE.SimLoadRecipeMapping . |
OrientationType | Returns or sets the orientation type of a NXOpen.CAE.SimLoadRecipeMapping . |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
SimLoadRecipeMappingOrientationTypes Enumeration | How the orientation of loads is mapped |
Property Detail¶
LoadType¶
-
SimLoadRecipeMapping.
LoadType
¶ Returns the load type of a
NXOpen.CAE.SimLoadRecipeMapping
.-------------------------------------
Getter Method
Signature
LoadType()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
OrientationType¶
-
SimLoadRecipeMapping.
OrientationType
¶ Returns or sets the orientation type of a
NXOpen.CAE.SimLoadRecipeMapping
.-------------------------------------
Getter Method
Signature
OrientationType()
Returns: Return type: NXOpen.CAE.SimLoadRecipeMappingOrientationTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationType(orientationType)
Parameters: orientationType ( NXOpen.CAE.SimLoadRecipeMappingOrientationTypes
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)