CaeGroupCollection Class¶
-
class
NXOpen.CAE.
CaeGroupCollection
¶ Bases:
object
Provides methods for managing set
NXOpen.CAE.CaeGroup
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CopyGroup | Copies the input group, which must come from the same part as the collection. |
CreateAutoGroups | Auto group CAE entities based on attributes Types (attribute types) by which auto grouping needs to be done should be specified using the JA CAE_GROUP_COLLECTION_auto_group_types structure. |
CreateExclusiveOrGroup | Create a XOR of Groups @return |
CreateGroup | Create a Group @return |
CreateGroupFromEntityIds | Create a Node/Element Group from node/element IDs @return |
CreateIntersectionGroup | Create a Intersection of Groups @return |
CreateOutputGroup | Create a Output Group @return |
CreateSubtractGroup | Create a Subtraction of two Groups @return |
CreateUnionGroup | Create a Union of Groups @return |
FindObject | Finds the NXOpen.CAE.CaeGroup with the given identifier as recorded in a journal. |
QueryGroupList | Query Groups list |
Enumerations¶
CaeGroupCollectionEntityType Enumeration | Entity type |
Structs¶
CaeGroupCollectionAutoGroupErrorCodes_Struct Struct | Contains list of error codes for each auto group type |
CaeGroupCollectionAutoGroupSeedNames_Struct Struct | Contains the prefix seed names to be given to auto created groups by type If a seed value is passed as NULL, then the auto created groups by that type will be given a default prefix List of default prefixes are as follows: MAT- for material_seed PPT- for ppt_seed Color- for color_seed XSECT- for section_seed LAM- for laminate seed DIM- for dimension seed FE_TYPE- for meshcolltype_seed |
CaeGroupCollectionAutoGroupTypes_Struct Struct | Contains information about the types by which we do auto grouping |
Method Detail¶
CopyGroup¶
-
CaeGroupCollection.
CopyGroup
¶ Copies the input group, which must come from the same part as the collection.
Signature
CopyGroup(setName, sourceGroup)
Parameters: - setName (str) – New group name, if no name is input or the input name is invalid, a name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- sourceGroup (
NXOpen.CAE.CaeGroup
) – must come from the same part as the collection
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateAutoGroups¶
-
CaeGroupCollection.
CreateAutoGroups
¶ Auto group CAE entities based on attributes Types (attribute types) by which auto grouping needs to be done should be specified using the JA CAE_GROUP_COLLECTION_auto_group_types structure.
The number of auto created groups and the array of auto created groups will be returned. Errors if any are returned by auto group type through the JA CAE_GROUP_COLLECTION_auto_group_error_codes structure.
Signature
CreateAutoGroups(autoGroupTypes, autoGroupSeeds)
Parameters: - autoGroupTypes (
NXOpen.CAE.CaeGroupCollectionAutoGroupTypes_Struct
) – types specifying which attributes to group by - autoGroupSeeds (
NXOpen.CAE.CaeGroupCollectionAutoGroupSeedNames_Struct
) – prefix seed names for auto created groups by type. If this argument is NULL or if any seed name is NULL, default prefixes are given
Returns: a tuple
Return type: A tuple consisting of (errorCodes, autoGroups). errorCodes is a
NXOpen.CAE.CaeGroupCollectionAutoGroupErrorCodes_Struct
. list of generated error codes for each auto group type autoGroups is a list ofNXOpen.CAE.CaeGroup
. output array of auto created groupsNew in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- autoGroupTypes (
CreateExclusiveOrGroup¶
-
CaeGroupCollection.
CreateExclusiveOrGroup
¶ Create a XOR of Groups
Signature
CreateExclusiveOrGroup(setName, objects)
Parameters: - setName (str) – Name of the exclusive or group. If no name is input or the input name is invalid, a name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- objects (list of
NXOpen.CAE.CaeGroup
) –
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateGroup¶
-
CaeGroupCollection.
CreateGroup
¶ Create a Group
Signature
CreateGroup(setName, objects)
Parameters: - setName (str) – Name of a Set NOTE: The full Unicode character set is not supported for this parameter.
- objects (list of
NXOpen.TaggedObject
) –
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateGroupFromEntityIds¶
-
CaeGroupCollection.
CreateGroupFromEntityIds
¶ Create a Node/Element Group from node/element IDs
Signature
CreateGroupFromEntityIds(setName, entityType, entityID)
Parameters: - setName (str) – Name of a Set NOTE: The full Unicode character set is not supported for this parameter.
- entityType (
NXOpen.CAE.CaeGroupCollectionEntityType
) – - entityID (list of int) –
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateIntersectionGroup¶
-
CaeGroupCollection.
CreateIntersectionGroup
¶ Create a Intersection of Groups
Signature
CreateIntersectionGroup(setName, objects)
Parameters: - setName (str) – Name of the Intersection group. If no name is input or the input name is invalid, a name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- objects (list of
NXOpen.CAE.CaeGroup
) –
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateOutputGroup¶
-
CaeGroupCollection.
CreateOutputGroup
¶ Create a Output Group
Signature
CreateOutputGroup(objects)
Parameters: objects (list of NXOpen.TaggedObject
) –Returns: Return type: NXOpen.CAE.CaeGroup
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateSubtractGroup¶
-
CaeGroupCollection.
CreateSubtractGroup
¶ Create a Subtraction of two Groups
Signature
CreateSubtractGroup(setName, fromGroup, excludedGroup)
Parameters: - setName (str) – Name of the subtraction group. If no name is input or the input name is invalid, a name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- fromGroup (
NXOpen.CAE.CaeGroup
) – The Set that will be substracted - excludedGroup (
NXOpen.CAE.CaeGroup
) – The Set that will be used for substraction
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateUnionGroup¶
-
CaeGroupCollection.
CreateUnionGroup
¶ Create a Union of Groups
Signature
CreateUnionGroup(setName, objects)
Parameters: - setName (str) – Name of the Union group. If no name is input or the input name is invalid, a name will be generated. NOTE: The full Unicode character set is not supported for this parameter.
- objects (list of
NXOpen.CAE.CaeGroup
) –
Returns: Return type: New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
CaeGroupCollection.
FindObject
¶ Finds the
NXOpen.CAE.CaeGroup
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier of the Set you want Returns: Return type: NXOpen.CAE.CaeGroup
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
QueryGroupList¶
-
CaeGroupCollection.
QueryGroupList
¶ Query Groups list
Signature
QueryGroupList()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)