ModelUpdateSolutionTargetType Enumeration¶
NXOpen.CAE.ModelUpdateSolution.TargetType is an alias for NXOpen.CAE.ModelUpdateSolutionTargetType
-
class
NXOpen.CAE.
ModelUpdateSolutionTargetType
¶ Bases:
object
Represents the type when export to targets and errors to csv file
Enum Members
Enum Member Enum Member Description All Export all the targets to the csv fileFrequencies Export all the frequency targets to the csv fileModeShapes Export all the mode shape targets to the csv file-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-