ModelUpdateOverallWeightsBuilder Class¶
-
class
NXOpen.CAE.
ModelUpdateOverallWeightsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelUpdateOverallWeightsBuilder
To create a new instance of this class, use
NXOpen.CAE.ModelUpdateSolution.CreateOverallWeightsBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Frequencies | Returns or sets the overall weights of frequency targets |
ModeShapes | Returns or sets the overall weights of mode shape targets |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Frequencies¶
-
ModelUpdateOverallWeightsBuilder.
Frequencies
¶ Returns or sets the overall weights of frequency targets
-------------------------------------
Getter Method
Signature
Frequencies()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Frequencies(frequencies)
Parameters: frequencies (float) – New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
ModeShapes¶
-
ModelUpdateOverallWeightsBuilder.
ModeShapes
¶ Returns or sets the overall weights of mode shape targets
-------------------------------------
Getter Method
Signature
ModeShapes()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModeShapes(modeShapes)
Parameters: modeShapes (float) – New in version NX7.5.0.
License requirements: nx_correl_update (“FE Model Update”)
Method Detail¶
Validate¶
-
ModelUpdateOverallWeightsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.