DurabilityEvaluateFatigueHistoryBuilder Class¶
-
class
NXOpen.CAE.
DurabilityEvaluateFatigueHistoryBuilder
¶ Bases:
NXOpen.Builder
Represents the builder for evaluating fatigue histories.
To create a new instance of this class, use
NXOpen.CAE.DurabilityManager.CreateDurabilityEvaluateFatigueHistoryBuilder
Default values.
Property Value FatigueHistoryDataType Stress New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
FatigueHistoryDataType | Returns or sets the fatigue history enum |
OutputAfuFileName | Returns or sets the output afu file name. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AfuFunction | The function is called when the user click the button of Export to AFU Funciton |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditEvent | The function is called when the user click the button of Edit Event Attributes |
ExportFatigueHistoryToCsv | Export fatigue history functions to a csv file. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DurabilityEvaluateFatigueHistoryBuilderFatigueHistoryDataTypeEnum Enumeration | Fatigue history data type: as per event, stress or strain |
Property Detail¶
FatigueHistoryDataType¶
-
DurabilityEvaluateFatigueHistoryBuilder.
FatigueHistoryDataType
¶ Returns or sets the fatigue history enum
-------------------------------------
Getter Method
Signature
FatigueHistoryDataType()
Returns: Return type: NXOpen.CAE.DurabilityEvaluateFatigueHistoryBuilderFatigueHistoryDataTypeEnum
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueHistoryDataType(fatigueHistoryDataType)
Parameters: fatigueHistoryDataType ( NXOpen.CAE.DurabilityEvaluateFatigueHistoryBuilderFatigueHistoryDataTypeEnum
) –New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OutputAfuFileName¶
-
DurabilityEvaluateFatigueHistoryBuilder.
OutputAfuFileName
¶ Returns or sets the output afu file name.
-------------------------------------
Getter Method
Signature
OutputAfuFileName()
Returns: Return type: str New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
-------------------------------------
Setter Method
Signature
OutputAfuFileName(filename)
Parameters: filename (str) – New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
AfuFunction¶
-
DurabilityEvaluateFatigueHistoryBuilder.
AfuFunction
¶ The function is called when the user click the button of Export to AFU Funciton
Signature
AfuFunction()
New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EditEvent¶
-
DurabilityEvaluateFatigueHistoryBuilder.
EditEvent
¶ The function is called when the user click the button of Edit Event Attributes
Signature
EditEvent()
New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
ExportFatigueHistoryToCsv¶
-
DurabilityEvaluateFatigueHistoryBuilder.
ExportFatigueHistoryToCsv
¶ Export fatigue history functions to a csv file.
Signature
ExportFatigueHistoryToCsv(csvFilename)
Parameters: csvFilename (str) – fatigue history functions will be written-out to this file. NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.1.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Validate¶
-
DurabilityEvaluateFatigueHistoryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.