LaminateDynamicSimCollection Class¶
-
class
NXOpen.CAE.
LaminateDynamicSimCollection
¶ Bases:
object
Represents a collection of laminate dynamic sims
To obtain an instance of this class, refer to
NXOpen.CAE.LaminateManager
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CloneDynamicSim | Clones the laminate dynamic sim |
CreateDampingFactorBuilder | Creates a builder for the laminate damping factor. |
CreateDynamicSimBuilder | Creates a builder for the laminate dynamic sim. |
Delete | Deletes the laminate dynamic sim |
FindObject | Finds a laminate dynamic sim with the specified name @return Laminate Dynamic Sim found |
Property Detail¶
Active¶
-
LaminateDynamicSimCollection.
Active
¶ Returns or sets the active laminate dynamic sim
-------------------------------------
Getter Method
Signature
Active()
Returns: Active laminate dynamic sim Return type: NXOpen.CAE.LaminateDynamicSim
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
-------------------------------------
Setter Method
Signature
Active(dynamicSim)
Parameters: dynamicSim ( NXOpen.CAE.LaminateDynamicSim
) – Laminate dynamic sim to be set activeNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Method Detail¶
CloneDynamicSim¶
-
LaminateDynamicSimCollection.
CloneDynamicSim
¶ Clones the laminate dynamic sim
Signature
CloneDynamicSim(dynamicSim)
Parameters: dynamicSim ( NXOpen.CAE.LaminateDynamicSim
) – Laminate dynamic sim to be clonedNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateDampingFactorBuilder¶
-
LaminateDynamicSimCollection.
CreateDampingFactorBuilder
¶ Creates a builder for the laminate damping factor.
Signature
CreateDampingFactorBuilder(contextObjectTag)
Parameters: contextObjectTag ( NXOpen.TaggedObject
) – The metasolution or the mode property.Returns: Return type: NXOpen.CAE.LaminateDampingFactorBuilder
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
CreateDynamicSimBuilder¶
-
LaminateDynamicSimCollection.
CreateDynamicSimBuilder
¶ Creates a builder for the laminate dynamic sim.
Signature
CreateDynamicSimBuilder(laminateDynamicSimTag)
Parameters: laminateDynamicSimTag ( NXOpen.CAE.LaminateDynamicSim
) – The metasolution.Returns: Return type: NXOpen.CAE.LaminateDynamicSimBuilder
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
Delete¶
-
LaminateDynamicSimCollection.
Delete
¶ Deletes the laminate dynamic sim
Signature
Delete(dynamicSim)
Parameters: dynamicSim ( NXOpen.CAE.LaminateDynamicSim
) – Laminate dynamic sim to be deletedNew in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FindObject¶
-
LaminateDynamicSimCollection.
FindObject
¶ Finds a laminate dynamic sim with the specified name
Signature
FindObject(name)
Parameters: name (str) – Laminate Dynamic Sim name to be found Returns: Laminate Dynamic Sim found Return type: NXOpen.CAE.LaminateDynamicSim
New in version NX9.0.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)