PostGraphBuilderGeometryValue Enumeration¶
NXOpen.CAE.PostGraphBuilder.GeometryValue is an alias for NXOpen.CAE.PostGraphBuilderGeometryValue
-
class
NXOpen.CAE.
PostGraphBuilderGeometryValue
¶ Bases:
object
This option is used to when the geometric entity selected has multiple result values.
This option applies to how we will resolve these multiple values into one
Enum Members
Enum Member Enum Member Description Average Minimum Maximum Sum WeightedAverage Integral -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-