ElementModifyTypeBuilder Class¶
-
class
NXOpen.CAE.
ElementModifyTypeBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ElementModifyTypeBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateElementModifyTypeBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ElementType | Returns the element type to be created |
MeshCollectorName | Returns or sets the mesh collector name |
MeshSelection | Returns the selected meshes |
Tag | Returns the Tag for this object. |
UseSourceMeshCollector | Returns or sets the option to use source mesh collector as a destination mesh collector |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ElementType¶
-
ElementModifyTypeBuilder.
ElementType
¶ Returns the element type to be created
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX8.5.0.
License requirements: None.
MeshCollectorName¶
-
ElementModifyTypeBuilder.
MeshCollectorName
¶ Returns or sets the mesh collector name
-------------------------------------
Getter Method
Signature
MeshCollectorName()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshCollectorName(meshCollectorName)
Parameters: meshCollectorName (str) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshSelection¶
-
ElementModifyTypeBuilder.
MeshSelection
¶ Returns the selected meshes
-------------------------------------
Getter Method
Signature
MeshSelection()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
UseSourceMeshCollector¶
-
ElementModifyTypeBuilder.
UseSourceMeshCollector
¶ Returns or sets the option to use source mesh collector as a destination mesh collector
-------------------------------------
Getter Method
Signature
UseSourceMeshCollector()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseSourceMeshCollector(useSourceMeshCollector)
Parameters: useSourceMeshCollector (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
ElementModifyTypeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.