CAESet Class¶
-
class
NXOpen.CAE.
CAESet
¶ Bases:
NXOpen.TransientObject
Represents a group of CAE object sets. The objects in each set can be used to create loads, constraints ..etc
To create a new instance of this class, use
NXOpen.CAE.SetManager.CreateCaeSet
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Destroys the set |
GetMembers | Gets the objects in the set. |
SetMembers | Sets the objects in the set. |
Method Detail¶
Dispose¶
-
CAESet.
Dispose
¶ Destroys the set
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetMembers¶
-
CAESet.
GetMembers
¶ Gets the objects in the set.
Signature
GetMembers()
Returns: objects in set Return type: list of NXOpen.CAE.SetObject
New in version NX4.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetMembers¶
-
CAESet.
SetMembers
¶ Sets the objects in the set.
Signature
SetMembers(members)
Parameters: members (list of NXOpen.CAE.SetObject
) – objects to add to setNew in version NX4.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)