GroupElemMethodElemOptionElemOption Enumeration¶
NXOpen.CAE.GroupElemMethodElemOption.ElemOption is an alias for NXOpen.CAE.GroupElemMethodElemOptionElemOption
-
class
NXOpen.CAE.
GroupElemMethodElemOptionElemOption
¶ Bases:
object
Used to specify the sub type of selected objects e.
g face of an element, edge of an element ..etc
Enum Members
Enum Member Enum Member Description ElemAll return all elements in the groupElem0d return 0D elements in the groupElem1d return 1D elements in the groupElem2d return 2D elements in the groupElem3d return 3D elements in the groupElemface2d return 2D elements in the group as element facesElemedge1d return 1D elements in the group as element edges-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-