BeamEADBuilder Class¶
-
class
NXOpen.CAE.
BeamEADBuilder
¶ Bases:
NXOpen.Builder
This class provides Beam/Bar Associated Data Support
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateBeamEadBuilder
Default values.
Property Value EndReleaseAState Ignore EndReleaseBState Ignore OrientationState Ignore New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the select element operator selects elements |
EndOffsetA1 | Returns the end A offset component 1 expression of the element |
EndOffsetA2 | Returns the end A offset component 2 expression of the element |
EndOffsetA3 | Returns the end A offset component 3 expression of the element |
EndOffsetAState | Returns or sets the state drives the commit action |
EndOffsetB1 | Returns the end B offset component 1 expression of the element |
EndOffsetB2 | Returns the end B offset component 2 expression of the element |
EndOffsetB3 | Returns the end B offset component 3 expression of the element |
EndOffsetBState | Returns or sets the state drives the commit action |
EndReleaseA1 | Returns or sets the get end release setting turns on or off the DOF 1 for end A |
EndReleaseA2 | Returns or sets the get end release setting turns on or off the DOF 2 for end A |
EndReleaseA3 | Returns or sets the get end release setting turns on or off the DOF 3 for end A |
EndReleaseA4 | Returns or sets the get end release setting turns on or off the DOF 4 for end A |
EndReleaseA5 | Returns or sets the get end release setting turns on or off the DOF 5 for end A |
EndReleaseA6 | Returns or sets the get end release setting turns on or off the DOF 6 for end A |
EndReleaseAState | Returns or sets the method to get the state of end release A |
EndReleaseB1 | Returns or sets the get end release setting turns on or off the DOF 1 for end B |
EndReleaseB2 | Returns or sets the get end release setting turns on or off the DOF 2 for end B |
EndReleaseB3 | Returns or sets the get end release setting turns on or off the DOF 3 for end B |
EndReleaseB4 | Returns or sets the get end release setting turns on or off the DOF 4 for end B |
EndReleaseB5 | Returns or sets the get end release setting turns on or off the DOF 5 for end B |
EndReleaseB6 | Returns or sets the get end release setting turns on or off the DOF 6 for end B |
EndReleaseBState | Returns or sets the method to get the state of end release B |
Node | Returns the get node operator selects an orientation node |
OriMethod | Returns or sets the method to get the element orientation method |
OrientationState | Returns or sets the state drives the commit action |
SelectSectionOri | Returns or sets the get selection ori operator gets section orientaion value |
Tag | Returns the Tag for this object. |
VectorChoice | Returns or sets the method to get the orientation vector choice |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BeamEADBuilderEndReleaseSetting Enumeration | indicates which end release setting to use |
BeamEADBuilderOrientationMethod Enumeration | indicates which orientation method to use |
BeamEADBuilderState Enumeration | indicates to ignore, apply or clear the state property upon commit |
BeamEADBuilderVectorChoiceType Enumeration | indicates which vector choice to use |
Property Detail¶
Elements¶
-
BeamEADBuilder.
Elements
¶ Returns the select element operator selects elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetA1¶
-
BeamEADBuilder.
EndOffsetA1
¶ Returns the end A offset component 1 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetA1()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetA2¶
-
BeamEADBuilder.
EndOffsetA2
¶ Returns the end A offset component 2 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetA2()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetA3¶
-
BeamEADBuilder.
EndOffsetA3
¶ Returns the end A offset component 3 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetA3()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetAState¶
-
BeamEADBuilder.
EndOffsetAState
¶ Returns or sets the state drives the commit action
-------------------------------------
Getter Method
Signature
EndOffsetAState()
Returns: Return type: NXOpen.CAE.BeamEADBuilderState
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndOffsetAState(endOffsetAState)
Parameters: endOffsetAState ( NXOpen.CAE.BeamEADBuilderState
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetB1¶
-
BeamEADBuilder.
EndOffsetB1
¶ Returns the end B offset component 1 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetB1()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetB2¶
-
BeamEADBuilder.
EndOffsetB2
¶ Returns the end B offset component 2 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetB2()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetB3¶
-
BeamEADBuilder.
EndOffsetB3
¶ Returns the end B offset component 3 expression of the element
-------------------------------------
Getter Method
Signature
EndOffsetB3()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndOffsetBState¶
-
BeamEADBuilder.
EndOffsetBState
¶ Returns or sets the state drives the commit action
-------------------------------------
Getter Method
Signature
EndOffsetBState()
Returns: Return type: NXOpen.CAE.BeamEADBuilderState
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndOffsetBState(endOffsetBState)
Parameters: endOffsetBState ( NXOpen.CAE.BeamEADBuilderState
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA1¶
-
BeamEADBuilder.
EndReleaseA1
¶ Returns or sets the get end release setting turns on or off the DOF 1 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA1()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA1(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA2¶
-
BeamEADBuilder.
EndReleaseA2
¶ Returns or sets the get end release setting turns on or off the DOF 2 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA2()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA2(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA3¶
-
BeamEADBuilder.
EndReleaseA3
¶ Returns or sets the get end release setting turns on or off the DOF 3 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA3()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA3(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA4¶
-
BeamEADBuilder.
EndReleaseA4
¶ Returns or sets the get end release setting turns on or off the DOF 4 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA4()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA4(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA5¶
-
BeamEADBuilder.
EndReleaseA5
¶ Returns or sets the get end release setting turns on or off the DOF 5 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA5()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA5(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseA6¶
-
BeamEADBuilder.
EndReleaseA6
¶ Returns or sets the get end release setting turns on or off the DOF 6 for end A
-------------------------------------
Getter Method
Signature
EndReleaseA6()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseA6(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseAState¶
-
BeamEADBuilder.
EndReleaseAState
¶ Returns or sets the method to get the state of end release A
-------------------------------------
Getter Method
Signature
EndReleaseAState()
Returns: Return type: NXOpen.CAE.BeamEADBuilderState
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseAState(endReleaseAState)
Parameters: endReleaseAState ( NXOpen.CAE.BeamEADBuilderState
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB1¶
-
BeamEADBuilder.
EndReleaseB1
¶ Returns or sets the get end release setting turns on or off the DOF 1 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB1()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB1(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB2¶
-
BeamEADBuilder.
EndReleaseB2
¶ Returns or sets the get end release setting turns on or off the DOF 2 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB2()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB2(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB3¶
-
BeamEADBuilder.
EndReleaseB3
¶ Returns or sets the get end release setting turns on or off the DOF 3 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB3()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB3(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB4¶
-
BeamEADBuilder.
EndReleaseB4
¶ Returns or sets the get end release setting turns on or off the DOF 4 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB4()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB4(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB5¶
-
BeamEADBuilder.
EndReleaseB5
¶ Returns or sets the get end release setting turns on or off the DOF 5 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB5()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB5(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseB6¶
-
BeamEADBuilder.
EndReleaseB6
¶ Returns or sets the get end release setting turns on or off the DOF 6 for end B
-------------------------------------
Getter Method
Signature
EndReleaseB6()
Returns: Return type: NXOpen.CAE.BeamEADBuilderEndReleaseSetting
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseB6(endReleaseSetting)
Parameters: endReleaseSetting ( NXOpen.CAE.BeamEADBuilderEndReleaseSetting
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
EndReleaseBState¶
-
BeamEADBuilder.
EndReleaseBState
¶ Returns or sets the method to get the state of end release B
-------------------------------------
Getter Method
Signature
EndReleaseBState()
Returns: Return type: NXOpen.CAE.BeamEADBuilderState
New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
EndReleaseBState(endReleaseBState)
Parameters: endReleaseBState ( NXOpen.CAE.BeamEADBuilderState
) –New in version NX6.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”)
Node¶
-
BeamEADBuilder.
Node
¶ Returns the get node operator selects an orientation node
-------------------------------------
Getter Method
Signature
Node()
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OriMethod¶
-
BeamEADBuilder.
OriMethod
¶ Returns or sets the method to get the element orientation method
-------------------------------------
Getter Method
Signature
OriMethod()
Returns: Return type: NXOpen.CAE.BeamEADBuilderOrientationMethod
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OriMethod(oriMethod)
Parameters: oriMethod ( NXOpen.CAE.BeamEADBuilderOrientationMethod
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
OrientationState¶
-
BeamEADBuilder.
OrientationState
¶ Returns or sets the state drives the commit action
-------------------------------------
Getter Method
Signature
OrientationState()
Returns: Return type: NXOpen.CAE.BeamEADBuilderState
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
OrientationState(orientationState)
Parameters: orientationState ( NXOpen.CAE.BeamEADBuilderState
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectSectionOri¶
-
BeamEADBuilder.
SelectSectionOri
¶ Returns or sets the get selection ori operator gets section orientaion value
-------------------------------------
Getter Method
Signature
SelectSectionOri()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
SelectSectionOri(selectSectionOri)
Parameters: selectSectionOri ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
VectorChoice¶
-
BeamEADBuilder.
VectorChoice
¶ Returns or sets the method to get the orientation vector choice
-------------------------------------
Getter Method
Signature
VectorChoice()
Returns: Return type: NXOpen.CAE.BeamEADBuilderVectorChoiceType
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
VectorChoice(vectorChoice)
Parameters: vectorChoice ( NXOpen.CAE.BeamEADBuilderVectorChoiceType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
BeamEADBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.