SimLoadRecipeSource Class¶
-
class
NXOpen.CAE.
SimLoadRecipeSource
¶ Bases:
NXOpen.TaggedObject
This is the class handling the attributes of a source used by a load recipe.
Use CAE.SimLoadRecipeSourceCollection.Create
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
FormatType | Returns or sets the format type of a NXOpen.CAE.SimLoadRecipeSource . |
Path | Returns or sets the path of a NXOpen.CAE.SimLoadRecipeSource . |
ReaderType | Returns or sets the reader type of a NXOpen.CAE.SimLoadRecipeSource . |
SourceLabel | Returns or sets the label of a NXOpen.CAE.SimLoadRecipeSource . |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetPropertyTable | Get the NXOpen.BasePropertyTable of a NXOpen.CAE.SimLoadRecipeSource @return |
Property Detail¶
FormatType¶
-
SimLoadRecipeSource.
FormatType
¶ Returns or sets the format type of a
NXOpen.CAE.SimLoadRecipeSource
.The available format types are declared in datasourcehandlers.xml file located in <ja_lt>NX_install_dir<ja_gt>/UGSTRUCTURES/cae_language directory.
This string correlates to the Name attribute of the FormatHandler elements.
-------------------------------------
Getter Method
Signature
FormatType()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FormatType(formatType)
Parameters: formatType (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Path¶
-
SimLoadRecipeSource.
Path
¶ Returns or sets the path of a
NXOpen.CAE.SimLoadRecipeSource
.-------------------------------------
Getter Method
Signature
Path()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Path(path)
Parameters: path (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReaderType¶
-
SimLoadRecipeSource.
ReaderType
¶ Returns or sets the reader type of a
NXOpen.CAE.SimLoadRecipeSource
.The available reader types are declared in datasourcehandlers.xml file located in <ja_lt>NX_install_dir<ja_gt>/UGSTRUCTURES/cae_language directory.
This string correlates to the Type attribute of the FileFormat elements.
-------------------------------------
Getter Method
Signature
ReaderType()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReaderType(readerType)
Parameters: readerType (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceLabel¶
-
SimLoadRecipeSource.
SourceLabel
¶ Returns or sets the label of a
NXOpen.CAE.SimLoadRecipeSource
.-------------------------------------
Getter Method
Signature
SourceLabel()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SourceLabel(sourceLabel)
Parameters: sourceLabel (str) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
GetPropertyTable¶
-
SimLoadRecipeSource.
GetPropertyTable
¶ Get the
NXOpen.BasePropertyTable
of aNXOpen.CAE.SimLoadRecipeSource
Signature
GetPropertyTable()
Returns: Return type: NXOpen.BasePropertyTable
New in version NX10.0.0.
License requirements: None.