CaeDataContainer Class¶
-
class
NXOpen.CAE.
CaeDataContainer
¶ Bases:
NXOpen.DataContainer
Represents a list of named properties, where the property name is a unique string.
The properties can be accessed and modified. In addition, new Properties can be added to the existing list.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Length | Returns the length of the list |
Mode | Returns the mode of the list |
Methods¶
Method | Description |
---|---|
AddBits | Adds the bits value in the container. |
AddDouble | Adds the double value in the container. |
AddDoubleMatrix | Adds the double matrix in the container. |
AddDoubleVector | Adds the double vector in the container. |
AddEnum | Adds the enum members in the container. |
AddFile | Adds the value in the container. |
AddInteger | Adds the integer value in the container. |
AddIntegerMatrix | Adds the integer matrix in the container. |
AddIntegerVector | Adds the integer vector in the container. |
AddLogical | Adds the logical value in the container. |
AddPoint | Adds the point value in the container. |
AddString | Adds the string value in the container. |
AddStrings | Adds the strings value in the container. |
AddTaggedObject | Adds the tagged object in the container. |
AddTaggedObjectVector | Adds the tagged object vector in the container. |
AddVector | Adds the vector value in the container. |
Dispose | Frees the object from memory. |
GetArray | Gets the value for the given property name. |
GetBits | Gets the bits value for the given property name. |
GetDouble | Gets the double value for the given property name. |
GetDoubleMatrix | Gets the double matrix for the given property name. |
GetDoubleVector | Gets the double vector for the given property name. |
GetEnum | Gets the value for the given property name. |
GetEnumAsString | Gets the value for the given property name. |
GetEnumMembers | Gets the enum members for the given property of type enum. |
GetFile | Gets the value for the given property name. |
GetInteger | Gets the integer value for the given property name. |
GetIntegerMatrix | Gets the integer matrix for the given property name. |
GetIntegerVector | Gets the integer vector for the given property name. |
GetLogical | Gets the logical value for the given property name. |
GetPoint | Gets the point value for the given property name. |
GetPropertyNames | Returns a list of all the property names @return Property names |
GetPropertyType | Returns the property type for given property name @return Property type. |
GetString | Gets the string value for the given property name. |
GetStrings | Gets the strings value for the given property name. |
GetTaggedObject | Gets the tagged object for the given property name. |
GetTaggedObjectVector | Gets the tagged object vector for the given property name. |
GetVector | Gets the vector value for the given property name. |
SetBits | Sets the bits value for the given property name. |
SetDouble | Sets the double value for the given property name. |
SetDoubleMatrix | Sets the double matrix for the given property name. |
SetDoubleVector | Sets the double vector for the given property name. |
SetEnum | Sets the value for the given property name. |
SetEnumAsString | Sets the value for the given property name. |
SetEnumMembers | Sets the enum members for the given property of type enum. |
SetFile | Sets the value for the given property name. |
SetInteger | Sets the integer value for the given property name. |
SetIntegerMatrix | Sets the integer matrix for the given property name. |
SetIntegerVector | Sets the integer vector for the given property name. |
SetLogical | Sets the logical value for the given property name. |
SetPoint | Sets the point value for the given property name. |
SetString | Sets the string value for the given property name. |
SetStrings | Sets the strings value for the given property name. |
SetTaggedObject | Sets the tagged object for the given property name. |
SetTaggedObjectVector | Sets the tagged object vector for the given property name. |
SetVector | Sets the vector value for the given property name. |