ElementTypeBuilderElementType Enumeration¶
NXOpen.CAE.ElementTypeBuilder.ElementType is an alias for NXOpen.CAE.ElementTypeBuilderElementType
-
class
NXOpen.CAE.
ElementTypeBuilderElementType
¶ Bases:
object
Dimension of the element types to be specified.
Enum Members
Enum Member Enum Member Description Point 0D elementBeam beamShell shellFreeSolid Free mesh solidSweepSolid Sweep mesh solidSweepSolidWedge Sweep mesh solid with wedgesSpider Spider ConnectionConnection ConnectionAnySolid Any solidTriaShell Tria shellQuadShell Quad shellWeld Weld elementContact Contact element-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-