LaminateGlobalLayupCollection Class¶
-
class
NXOpen.CAE.
LaminateGlobalLayupCollection
¶ Bases:
object
Represents a global layup, which is defined by a sequence of
NXOpen.CAE.LaminateGlobalLayup
, each with a name and a list of pliesTo obtain an instance of this class, refer to
NXOpen.CAE.LaminateGlobalLayupMgr
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateGlobalLayup | Create a new NXOpen.CAE.LaminateGlobalLayup instance @return |
DeleteGlobalLayup | Delete an existing NXOpen.CAE.LaminateGlobalLayup instance |
FindObject | Finds the NXOpen.CAE.LaminateGlobalLayup with the given identifier as recorded in a journal. |
Method Detail¶
CreateGlobalLayup¶
-
LaminateGlobalLayupCollection.
CreateGlobalLayup
¶ Create a new
NXOpen.CAE.LaminateGlobalLayup
instanceSignature
CreateGlobalLayup()
Returns: Return type: NXOpen.CAE.LaminateGlobalLayup
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
DeleteGlobalLayup¶
-
LaminateGlobalLayupCollection.
DeleteGlobalLayup
¶ Delete an existing
NXOpen.CAE.LaminateGlobalLayup
instanceSignature
DeleteGlobalLayup(layupToRemove)
Parameters: layupToRemove ( NXOpen.CAE.LaminateGlobalLayup
) –New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)
FindObject¶
-
LaminateGlobalLayupCollection.
FindObject
¶ Finds the
NXOpen.CAE.LaminateGlobalLayup
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: global layup found Return type: NXOpen.CAE.LaminateGlobalLayup
New in version NX7.5.0.
License requirements: nx_lam_comp_adv (“Laminate Composites Advanced”)