CorrelAlignmentBuilderReferencePt_Struct Struct¶
NXOpen.CAE.CorrelAlignmentBuilder.ReferencePt is an alias for NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct
-
class
NXOpen.CAE.
CorrelAlignmentBuilderReferencePt_Struct
¶ Bases:
object
Specifies the data for the selected reference points
Fields¶
Field | Description |
---|---|
Defined | |
NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct.X | |
NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct.Y | |
NXOpen.CAE.CorrelAlignmentBuilderReferencePt_Struct.Z | Point Coordinate |
Defined¶
-
CorrelAlignmentBuilderReferencePt_Struct.
Defined
¶ -------------------------------------
Getter Method Signature
Defined()
Returns: Return type: bool -------------------------------------
Setter Method
Signature
Defined(value)
Parameters: value (bool) –
X¶
-
CorrelAlignmentBuilderReferencePt_Struct.
X
¶ -------------------------------------
Getter Method Signature
X()
Returns: Return type: float -------------------------------------
Setter Method
Signature
X(value)
Parameters: value (float) –