AfuAbscissaHeaderInfo Class¶
-
class
NXOpen.CAE.
AfuAbscissaHeaderInfo
¶ Bases:
NXOpen.TransientObject
Represents the data to define abscissa header information for an afu record
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AxisLabel | Returns or sets the customized axis label |
Spacing | Returns or sets the value of spacing |
UnitLabel | Returns or sets the customized unit label |
Property Detail¶
AxisLabel¶
-
AfuAbscissaHeaderInfo.
AxisLabel
¶ Returns or sets the customized axis label
-------------------------------------
Getter Method
Signature
AxisLabel()
Returns: the customized axis label . Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
AxisLabel(axisLabel)
Parameters: axisLabel (str) – the customized axis label . Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Spacing¶
-
AfuAbscissaHeaderInfo.
Spacing
¶ Returns or sets the value of spacing
-------------------------------------
Getter Method
Signature
Spacing()
Returns: the value of spacing Return type: int New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
Spacing(spacing)
Parameters: spacing (int) – the value of spacing New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
UnitLabel¶
-
AfuAbscissaHeaderInfo.
UnitLabel
¶ Returns or sets the customized unit label
-------------------------------------
Getter Method
Signature
UnitLabel()
Returns: the customized unit label. Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
-------------------------------------
Setter Method
Signature
UnitLabel(unitLabel)
Parameters: unitLabel (str) – the customized unit label. Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)