MMCCreateBuilder Class¶
-
class
NXOpen.CAE.
MMCCreateBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.MMCCreateBuilder
which can be used to create or editNXOpen.CAE.MeshMate
objects.To create a new instance of this class, use
NXOpen.CAE.MeshControlCollection.CreateMmcCreateBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AutoSelection | Returns the bodies/faces used when NXOpen.CAE.MMCCreateBuilder.Type is set to NXOpen.CAE.MMCCreateBuilderTypes.AutoCreate . |
DistTolerance | Returns the dist tolerance |
FaceSearchOption | Returns or sets the face search option |
MeshMatingOption | Returns or sets the mesh mating type |
Mmc | Returns or sets the Mesh Mating Condition |
ReverseDirection | Returns or sets the reverse direction |
SourceFace | Returns the source face used when NXOpen.CAE.MMCCreateBuilder.Type is set to NXOpen.CAE.MMCCreateBuilderTypes.Manual . |
Tag | Returns the Tag for this object. |
TargetFace | Returns the target face used when NXOpen.CAE.MMCCreateBuilder.Type is set to NXOpen.CAE.MMCCreateBuilderTypes.Manual . |
Type | Returns or sets the mmc creation type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitMmcs | Commits the creation of the NXOpen.CAE.MeshMate objects or Commits the changes made to the NXOpen.CAE.MeshMate @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MMCCreateBuilderFaceSearchType Enumeration | Types of Face Serach Operations |
MMCCreateBuilderMeshMatingType Enumeration | Types of Mesh Mating Conditions |
MMCCreateBuilderTypes Enumeration | Type of the Creation Methods for MMC |
Property Detail¶
AutoSelection¶
-
MMCCreateBuilder.
AutoSelection
¶ Returns the bodies/faces used when
NXOpen.CAE.MMCCreateBuilder.Type
is set toNXOpen.CAE.MMCCreateBuilderTypes.AutoCreate
.-------------------------------------
Getter Method
Signature
AutoSelection()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.5.
License requirements: None.
DistTolerance¶
-
MMCCreateBuilder.
DistTolerance
¶ Returns the dist tolerance
-------------------------------------
Getter Method
Signature
DistTolerance()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
FaceSearchOption¶
-
MMCCreateBuilder.
FaceSearchOption
¶ Returns or sets the face search option
-------------------------------------
Getter Method
Signature
FaceSearchOption()
Returns: Return type: NXOpen.CAE.MMCCreateBuilderFaceSearchType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceSearchOption(faceSearchOption)
Parameters: faceSearchOption ( NXOpen.CAE.MMCCreateBuilderFaceSearchType
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MeshMatingOption¶
-
MMCCreateBuilder.
MeshMatingOption
¶ Returns or sets the mesh mating type
-------------------------------------
Getter Method
Signature
MeshMatingOption()
Returns: Return type: NXOpen.CAE.MMCCreateBuilderMeshMatingType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeshMatingOption(meshMatingOption)
Parameters: meshMatingOption ( NXOpen.CAE.MMCCreateBuilderMeshMatingType
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Mmc¶
-
MMCCreateBuilder.
Mmc
¶ Returns or sets the Mesh Mating Condition
-------------------------------------
Getter Method
Signature
Mmc()
Returns: Return type: NXOpen.CAE.MeshMate
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mmc(mmc)
Parameters: mmc ( NXOpen.CAE.MeshMate
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReverseDirection¶
-
MMCCreateBuilder.
ReverseDirection
¶ Returns or sets the reverse direction
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SourceFace¶
-
MMCCreateBuilder.
SourceFace
¶ Returns the source face used when
NXOpen.CAE.MMCCreateBuilder.Type
is set toNXOpen.CAE.MMCCreateBuilderTypes.Manual
.-------------------------------------
Getter Method
Signature
SourceFace()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
TargetFace¶
-
MMCCreateBuilder.
TargetFace
¶ Returns the target face used when
NXOpen.CAE.MMCCreateBuilder.Type
is set toNXOpen.CAE.MMCCreateBuilderTypes.Manual
.-------------------------------------
Getter Method
Signature
TargetFace()
Returns: Return type: NXOpen.SelectIParameterizedSurface
New in version NX6.0.0.
License requirements: None.
Type¶
-
MMCCreateBuilder.
Type
¶ Returns or sets the mmc creation type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAE.MMCCreateBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.CAE.MMCCreateBuilderTypes
) –New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
CommitMmcs¶
-
MMCCreateBuilder.
CommitMmcs
¶ Commits the creation of the
NXOpen.CAE.MeshMate
objects or Commits the changes made to theNXOpen.CAE.MeshMate
Signature
CommitMmcs()
Returns: Return type: list of NXOpen.CAE.MeshMate
New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
MMCCreateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.