XyFunctionResponseType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionResponseType
¶ Bases:
object
Defines response purpose type of a function Enum Members
Enum Member Enum Member Description General Function is General Function.Time Function is Time HistorySpectrum Function is SpectrumPowerSpectralDensity Function is Power Spectral DensityShockResponseSpectrum Function is Shock Response SpectrumFrequencyResponseFunction Function is Frequency Response FunctionCrossSpectrum Function is Cross SpectrumTransmissibility Function is Transmissibility-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-