MappedMeshBuilder Class¶
-
class
NXOpen.CAE.
MappedMeshBuilder
¶ Bases:
NXOpen.Builder
Represents a Mapped Mesh Builder.
Used to create a
NXOpen.CAE.MappedMesh
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateMappedMeshBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
EccAuto | Returns or sets the ECC automatic mode option |
EccName | Returns or sets the ECC name |
EdgeMatchOption | Returns or sets the edge match toggle |
EdgeMatchTolerance | Returns or sets the edge match tolerance |
EdgeMergeAngle | Returns or sets the edge merge angle |
ElementSize | Returns or sets the element size |
ElementSizeExpression | Returns the element size |
ElementType | Returns or sets the elem type name. |
FlipDiagonals | Returns or sets the flip diagonals option |
FormatMesh | Returns or sets the format mesh option |
Jacobian | Returns or sets the jacobian |
KeepFreeMeshes | Returns or sets the keep free meshes option |
MergeEdges | Returns or sets the merge edges option |
MidNodeOption | Returns or sets the mid node opt |
ProjectVertices | Returns or sets the project vertices option |
QuadOnlyMesh | Returns or sets the quad only mesh option |
SelectionFace | Returns the selection face |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AutoSize | Auto-generated element size @return |
ChangeEdgeDensity | Returns the edge density |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerData | Returns the corner data @return |
GetObject | Returns the object currently being edited by this builder. |
PreviewMesh | Previews the mapped mesh for further edit. |
SetCornerData | Sets the corner data. |
SetCornerDataWithEdges | Sets the corner data using array of edges and int array consists of if user want start of an edge or an end of an edge. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MappedMeshBuilderMidNodeType Enumeration | Mid-node placement options |
Property Detail¶
EccAuto¶
-
MappedMeshBuilder.
EccAuto
¶ Returns or sets the ECC automatic mode option
-------------------------------------
Getter Method
Signature
EccAuto()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EccAuto(eccAutoOption)
Parameters: eccAutoOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EccName¶
-
MappedMeshBuilder.
EccName
¶ Returns or sets the ECC name
-------------------------------------
Getter Method
Signature
EccName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EccName(eccName)
Parameters: eccName (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeMatchOption¶
-
MappedMeshBuilder.
EdgeMatchOption
¶ Returns or sets the edge match toggle
-------------------------------------
Getter Method
Signature
EdgeMatchOption()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeMatchOption(edgeMatchOption)
Parameters: edgeMatchOption (bool) – New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeMatchTolerance¶
-
MappedMeshBuilder.
EdgeMatchTolerance
¶ Returns or sets the edge match tolerance
-------------------------------------
Getter Method
Signature
EdgeMatchTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeMatchTolerance(edgeMatchTolerance)
Parameters: edgeMatchTolerance (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeMergeAngle¶
-
MappedMeshBuilder.
EdgeMergeAngle
¶ Returns or sets the edge merge angle
-------------------------------------
Getter Method
Signature
EdgeMergeAngle()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeMergeAngle(edgeMergeAngle)
Parameters: edgeMergeAngle (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementSize¶
-
MappedMeshBuilder.
ElementSize
¶ Returns or sets the element size
-------------------------------------
Getter Method
Signature
ElementSize()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementSize(elementSize)
Parameters: elementSize (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementSizeExpression¶
-
MappedMeshBuilder.
ElementSizeExpression
¶ Returns the element size
-------------------------------------
Getter Method
Signature
ElementSizeExpression()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ElementType¶
-
MappedMeshBuilder.
ElementType
¶ Returns or sets the elem type name.
This name is solver environment dependent. These are the same names that show up in the meshing dialogues. Refer to the release specific CAE user documentation to set a specific element name desired for a specific solver environment in a given release, refer to the release specific user manual
-------------------------------------
Getter Method
Signature
ElementType()
Returns: Return type: str New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Setter Method
Signature
ElementType(typeOfElement)
Parameters: typeOfElement (str) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FlipDiagonals¶
-
MappedMeshBuilder.
FlipDiagonals
¶ Returns or sets the flip diagonals option
-------------------------------------
Getter Method
Signature
FlipDiagonals()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipDiagonals(flipDiagonalsOption)
Parameters: flipDiagonalsOption (bool) – New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FormatMesh¶
-
MappedMeshBuilder.
FormatMesh
¶ Returns or sets the format mesh option
-------------------------------------
Getter Method
Signature
FormatMesh()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FormatMesh(formatMeshOption)
Parameters: formatMeshOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Jacobian¶
-
MappedMeshBuilder.
Jacobian
¶ Returns or sets the jacobian
-------------------------------------
Getter Method
Signature
Jacobian()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Jacobian(jacobian)
Parameters: jacobian (float) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
KeepFreeMeshes¶
-
MappedMeshBuilder.
KeepFreeMeshes
¶ Returns or sets the keep free meshes option
-------------------------------------
Getter Method
Signature
KeepFreeMeshes()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepFreeMeshes(quadOnlyMeshOption)
Parameters: quadOnlyMeshOption (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MergeEdges¶
-
MappedMeshBuilder.
MergeEdges
¶ Returns or sets the merge edges option
-------------------------------------
Getter Method
Signature
MergeEdges()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MergeEdges(mergeEdgesOption)
Parameters: mergeEdgesOption (bool) – New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
MidNodeOption¶
-
MappedMeshBuilder.
MidNodeOption
¶ Returns or sets the mid node opt
-------------------------------------
Getter Method
Signature
MidNodeOption()
Returns: Return type: NXOpen.CAE.MappedMeshBuilderMidNodeType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MidNodeOption(midNodeType)
Parameters: midNodeType ( NXOpen.CAE.MappedMeshBuilderMidNodeType
) –New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ProjectVertices¶
-
MappedMeshBuilder.
ProjectVertices
¶ Returns or sets the project vertices option
-------------------------------------
Getter Method
Signature
ProjectVertices()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectVertices(projectVerticesOption)
Parameters: projectVerticesOption (bool) – New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
QuadOnlyMesh¶
-
MappedMeshBuilder.
QuadOnlyMesh
¶ Returns or sets the quad only mesh option
-------------------------------------
Getter Method
Signature
QuadOnlyMesh()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QuadOnlyMesh(quadOnlyMeshOption)
Parameters: quadOnlyMeshOption (bool) – New in version NX6.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectionFace¶
-
MappedMeshBuilder.
SelectionFace
¶ Returns the selection face
-------------------------------------
Getter Method
Signature
SelectionFace()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX5.0.0.
License requirements: None.
Method Detail¶
AutoSize¶
-
MappedMeshBuilder.
AutoSize
¶ Auto-generated element size
Signature
AutoSize()
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ChangeEdgeDensity¶
-
MappedMeshBuilder.
ChangeEdgeDensity
¶ Returns the edge density
Signature
ChangeEdgeDensity(edge, numberElements)
Parameters: - edge (
NXOpen.NXObject
) – - numberElements (int) –
New in version NX5.0.0.
License requirements: None.
- edge (
GetCornerData¶
-
MappedMeshBuilder.
GetCornerData
¶ Returns the corner data
Signature
GetCornerData()
Returns: a tuple Return type: A tuple consisting of (vertexList, face). vertexList is a list of NXOpen.NXObject
. face is aNXOpen.NXObject
.New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PreviewMesh¶
-
MappedMeshBuilder.
PreviewMesh
¶ Previews the mapped mesh for further edit.
After preview, corner definition is allowed.
Signature
PreviewMesh()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SetCornerData¶
-
MappedMeshBuilder.
SetCornerData
¶ Sets the corner data.
Signature
SetCornerData(face, vertexList)
Parameters: - face (
NXOpen.NXObject
) – - vertexList (list of
NXOpen.NXObject
) –
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- face (
SetCornerDataWithEdges¶
-
MappedMeshBuilder.
SetCornerDataWithEdges
¶ Sets the corner data using array of edges and int array consists of if user want start of an edge or an end of an edge.
This start of an edge map to the edge where 1 is start of an edge and 0 is end of an edge
Signature
SetCornerDataWithEdges(face, start, edge)
Parameters: - face (
NXOpen.NXObject
) – - start (list of int) –
- edge (list of
NXOpen.NXObject
) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
- face (
Validate¶
-
MappedMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.