BaseLoadcase Class¶
-
class
NXOpen.CAE.
BaseLoadcase
¶ Bases:
NXOpen.TaggedObject
This class provides interfaces to query loadcase attributes
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Name | Returns the NX assigned name of the loadcase |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Find | Returns a NXOpen.CAE.BaseIteration @return |
GetIterations | Get iteration present in this loadcase @return |
Property Detail¶
Method Detail¶
Find¶
-
BaseLoadcase.
Find
¶ Returns a
NXOpen.CAE.BaseIteration
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX7.5.0.
License requirements: None.
GetIterations¶
-
BaseLoadcase.
GetIterations
¶ Get iteration present in this loadcase
Signature
GetIterations()
Returns: Return type: list of NXOpen.CAE.BaseIteration
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)