OneDimensionalElementSplitBuilder Class¶
-
class
NXOpen.CAE.
OneDimensionalElementSplitBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.OneDimensionalElementSplitBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateOneDimensionalElementSplitBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Elements | Returns the selected elements |
LengthOfSubElements | Returns the length of sub elements |
NumberOfSubElements | Returns or sets the number of sub elements |
SplitMethod | Returns or sets the split method type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
OneDimensionalElementSplitBuilderSplitMethodType Enumeration | represents the split method types |
Property Detail¶
Elements¶
-
OneDimensionalElementSplitBuilder.
Elements
¶ Returns the selected elements
-------------------------------------
Getter Method
Signature
Elements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX8.5.0.
License requirements: None.
LengthOfSubElements¶
-
OneDimensionalElementSplitBuilder.
LengthOfSubElements
¶ Returns the length of sub elements
-------------------------------------
Getter Method
Signature
LengthOfSubElements()
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
NumberOfSubElements¶
-
OneDimensionalElementSplitBuilder.
NumberOfSubElements
¶ Returns or sets the number of sub elements
-------------------------------------
Getter Method
Signature
NumberOfSubElements()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfSubElements(numberOfSubElements)
Parameters: numberOfSubElements (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SplitMethod¶
-
OneDimensionalElementSplitBuilder.
SplitMethod
¶ Returns or sets the split method type
-------------------------------------
Getter Method
Signature
SplitMethod()
Returns: Return type: NXOpen.CAE.OneDimensionalElementSplitBuilderSplitMethodType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitMethod(option)
Parameters: option ( NXOpen.CAE.OneDimensionalElementSplitBuilderSplitMethodType
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
OneDimensionalElementSplitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.