ShowHideManager Class¶
-
class
NXOpen.CAE.
ShowHideManager
¶ Bases:
object
Provides method for creating builder for Show Hide operation commands in a fem/sim part
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateShowAdjacentBuilder | Creates a builder for Show Adjacent Command @return |
CreateShowHideBuilder | Creates a builder for Show Hide Command @return |
CreateShowOnlyBuilder | Creates a builder for Show Only Command @return |
ReverseFaceDisplay | Creates a builder for the Reverse Face Display Command, which reverses the display of each CAE geometry face in the model. |
Method Detail¶
CreateShowAdjacentBuilder¶
-
ShowHideManager.
CreateShowAdjacentBuilder
¶ Creates a builder for Show Adjacent Command
Signature
CreateShowAdjacentBuilder()
Returns: Return type: NXOpen.CAE.ShowAdjacentBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateShowHideBuilder¶
-
ShowHideManager.
CreateShowHideBuilder
¶ Creates a builder for Show Hide Command
Signature
CreateShowHideBuilder()
Returns: Return type: NXOpen.CAE.ShowHideBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
CreateShowOnlyBuilder¶
-
ShowHideManager.
CreateShowOnlyBuilder
¶ Creates a builder for Show Only Command
Signature
CreateShowOnlyBuilder()
Returns: Return type: NXOpen.CAE.ShowOnlyBuilder
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
ReverseFaceDisplay¶
-
ShowHideManager.
ReverseFaceDisplay
¶ Creates a builder for the Reverse Face Display Command, which reverses the display of each CAE geometry face in the model.
Use this method associated with
JA_SHOW_HIDE_MANAGER_create_show_only_builder
to examine the CAE model visually. For example, use the show only to visually check the a BC’s target sets, and then use reverse face display to visually examine the CAE geometry which doesn’t have this BC defined on it.Signature
ReverseFaceDisplay()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)