ResultType Class¶
-
class
NXOpen.CAE.
ResultType
¶ Bases:
NXOpen.CAE.BaseResultType
This class represents a result type from a result file.
The attributes of this object reflect what is present in the result file. This object can not be created externally as these cases comes from the result file it will be created automatically during result file loading
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Complex | Returns a value indicating whether the result type is a complex value |
Datatype | Returns the NXOpen.CAE.ResultDataType for this result type |
Location | Returns the NXOpen.CAE.ResultLocation where this result type is defined |
Name | Returns the name for this result type |
Quantity | Returns the NXOpen.CAE.ResultQuantity for this result type |
Subtitle | Returns the subtitle defined for the result type in the result file |
Tag | Returns the Tag for this object. |
Title | Returns the title defined for the result type in the result file |
UserName | Returns or sets the user defined name of this result type |
Methods¶
Method | Description |
---|---|
AskComponents | Return all results components available for this result type @return |
GetSectionDefined | Returns the sections where this result is defined. |
Property Detail¶
Subtitle¶
-
ResultType.
Subtitle
¶ Returns the subtitle defined for the result type in the result file
-------------------------------------
Getter Method
Signature
Subtitle()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Title¶
-
ResultType.
Title
¶ Returns the title defined for the result type in the result file
-------------------------------------
Getter Method
Signature
Title()
Returns: Return type: str New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)